LinkSoul Agent SDK (Python v1.5.0-SNAPSHOT)
LinkSoul Agent SDK (Python v1.5.0-SNAPSHOT)
🆕 v1.5.0 new capability: beyond-line-of-sight Teleop
⚠️ Not yet released: in-development v1.5.0-SNAPSHOT capability; interface and protocol may change. Do not use in production before the official release.
A third interaction path on top of passive / active — a remote operator drives the robot via
TeleopRequest.enter → start_audio(param) → append_audio_delta* → done_audio → exit.
- New class:
TeleopRequest(enter/start_audio(param=None)/append_audio_delta/done_audio/exit)- New callback bases:
TeleopEnterCallback.on_enter_ack/TeleopExitCallback.on_exit_ack- New
AgentSdkmethods:register_teleop(...)/unregister_teleop(teleop_id)- New policy:
AgentPolicy.TELEOP(wire value"teleop")- Seven new event types under
AGENTSDK_TELEOP_*; new ID prefixteleop_...start_audio(param)acceptsrole(man/woman),threshold(-14 – 14) for voice / VAD tuningSee the Teleop guide, Teleop API, and Teleop example.
🆕 v1.5.0 new capability: ExtSkill (Extended Skills)
⚠️ Not yet released: in-development v1.5.0-SNAPSHOT capability; interface and protocol may change. Do not use in production before the official release.
A new interaction path for querying the robot's available skill list and remotely invoking a specific skill (three-phase acknowledgement: ack → state → result):
- New class:
ExtSkillRequest(query/invoke)- New callback bases:
ExtSkillQueryCallback.on_query_result/ExtSkillInvokeCallback(on_invoke_ack+on_invoke_result)- New
AgentSdkmethods:register_ext_skill(...)/unregister_ext_skill(request_id)- New policy:
AgentPolicy.EXT_SKILL(wire value"extskill")- Five new event types under
AGENTSDK_EXT_SKILL_*; new ID prefixextskill_...See the ExtSkill guide, ExtSkill API, and ExtSkill example.
⚠️ v1.4.0 breaking auth change — NOT compatible with v1.3.0 or earlier
v1.4.0 standardises the AgentSDK signing scheme to align with the LinkSoul open-platform spec. v1.5.0 inherits the same signing scheme, so v1.3.0 (and earlier) clients still cannot upgrade in place:
- Auth: JWT (one
AGIBOT_AUTHORIZATIONheader) → HMAC-SHA256 with five signed headers (X-App-Id/X-App-Key/X-Timestamp/X-Nonce/X-Signature)- Credentials: legacy custom-agent template → application on the LinkSoul open platform (issues a new
app_keyalongsideapp_id/app_secret)- Factory:
AgentSdk.create(url, app_id, app_secret)→AgentSdk.create(url, app_id, app_key, app_secret)- Gateway URL:
wss://agentsdk.agibot.com/v1/agentsdk→wss://open.agibot.com/api/V1/open-portal/app/wss/agent-sdkcallback_typesmoves out of the JWT payload into a standaloneX-Callback-Typesheader (JSON array string)Upgrading requires rotating credentials, switching the gateway URL, updating the
create()call, and rewriting any custom auth-header handling. See the CHANGELOG for the full migration path.
Connection info
| Item | Value |
|---|---|
| WebSocket URL | wss://open.agibot.com/api/V1/open-portal/app/wss/agent-sdk |
| appId | Obtained from the LinkSoul open platform when creating an application |
| appKey | Obtained from the LinkSoul open platform when creating an application |
| appSecret | Obtained from the LinkSoul open platform when creating an application (HMAC-SHA256 signing key) |
from linksoul_agentsdk import AgentSdk
agent_sdk = AgentSdk.create(
url="wss://open.agibot.com/api/V1/open-portal/app/wss/agent-sdk",
app_id=app_id,
app_key="<your appKey>",
app_secret=app_secret,
)
Quick navigation
| Document | Description |
|---|---|
| Quick Start | 5-minute setup, pip install + full integration code |
| Architecture | System architecture, threading model, reconnect |
| Passive Callbacks Guide | 8 passive callback types + response methods |
| Robot-side state modules | All 22 state_name modules received in on_state, field schemas + frequency conventions |
| Active Operations Guide | Task flow (v1.3.0 first opened the active surface but only task flow was ever functional; v1.4.0 removes the never-enabled entries — skill / state query, pull / push stream — and narrows the public API to task flow) |
| Teleop Guide | New in v1.5.0: remote-operator teleop (enter → audio → exit) |
| ExtSkill Guide | New in v1.5.0: query available skills and invoke remotely (query / invoke, three-phase ack) |
| Task-flow payload protocol | Skill orchestration — action_group / action_type JSON reference + SIMPLE/COMPLEX examples |
| Semantic Skills | Full catalogue dispatched via response.on_skill or task flow |
| AgentSdk API | Main entry class full reference |
| Enums Reference | Every enum & value |
| Passive Callbacks API | Callback / Response signatures |
| Active Requests API | Task flow API |
| Teleop API | New in v1.5.0: TeleopRequest / callbacks |
| ExtSkill API | New in v1.5.0: ExtSkillRequest / ExtSkillQueryCallback / ExtSkillInvokeCallback |
| Passive Examples | Full passive-flow code |
| Active Examples | Full active-flow code |
| Teleop Example | New in v1.5.0: end-to-end teleop walkthrough |
| ExtSkill Example | New in v1.5.0: end-to-end ExtSkill query + invoke walkthrough |
| Troubleshooting & FAQ | Troubleshooting manual + FAQ (grows over time) |
| Error Handling & Operations | Error codes, reconnection, resource release, logging & troubleshooting |
| Glossary | Business / SDK / model / reject terminology reference |
| Changelog | Per-version changes |
Three interaction modes
LinkskyGatewayis the LinkSoul open-platform ingress gateway (wss://open.agibot.com/api/V1/open-portal/app/wss/agent-sdk); it relays bidirectional messages between the SDK and robots.
┌──────────────────────────────────────────────────────────────┐
│ LinkSoul Platform │
├──────────────────────────────────────────────────────────────┤
│ │
│ Robot ──Audio/Video/Text──→ LinkskyGateway ──→ SDK CB │ Passive
│ Robot ←──ASR/LLM/TTS────── LinkskyGateway ←── SDK Resp │
│ │
│ SDK Request ──→ LinkskyGateway ──→ Robot │ Active
│ SDK Result ←── LinkskyGateway ←── Robot │
│ │
│ Operator audio ──→ LinkskyGateway ──→ Robot │ Teleop (new in v1.5.0)
│ Operator ←──enter/exit ack── LinkskyGateway ←── Robot │
│ │
└──────────────────────────────────────────────────────────────┘
- Passive: robot initiates (audio/video/text) → SDK processes → returns ASR/LLM/VLM/TTS
- Active: SDK initiates → v1.3.0 first opened skill / state query, pull / push stream and task flow at the API level, but only task flow was ever functional; v1.4.0 removes those never-enabled entries and narrows the public surface to task flow
- Teleop (new in v1.5.0): a remote operator opens a session (
enter), streams audio (start_audio→append_audio_delta→done_audio), then closes withexit;enter/exitare ack'd via callback, audio events are fire-and-forget - ExtSkill (new in v1.5.0): the SDK queries the robot's available skill list (
query) and invokes a specific skill (invoke); invoke uses three-phase acknowledgement (ack → state → result); policy:AgentPolicy.EXT_SKILL
Distribution downloads
Direct downloads for offline / air-gapped integration:
| File | Kind | Size |
|---|---|---|
linksoul_agentsdk-1.5.0a1-py3-none-any.whl | wheel (recommended) | 68 KB |
linksoul_agentsdk-1.5.0a1.tar.gz | sdist (source distribution) | 70 KB |
# install the wheel
pip install ./linksoul_agentsdk-1.5.0a1-py3-none-any.whl
# or install from sdist
pip install ./linksoul_agentsdk-1.5.0a1.tar.gz
websocket-client>=1.7.0 is pulled in automatically (declared in the wheel METADATA). The 1.5.0a1 version string is the PEP 440 alpha pre-release identifier and is aligned with the Java SDK's 1.5.0-SNAPSHOT. See Quick Start for the detailed install flow.