Error Handling & Operations
Error Handling & Operations
Auto-Reconnect Mechanism
The SDK has built-in auto-reconnect; no developer handling is needed:
| Feature | Behavior |
|---|---|
| Connection lost | Auto-reconnect with 3-second delay |
| Retry count | Infinite retries (until release() is called) |
| Heartbeat | Ping sent every 10 seconds |
| Token refresh | New JWT generated on each reconnect (1-hour validity) |
| After reconnection | Robot will resend online events |
Auth Callback
java
agentSdk.registerAuth((appId, code, msg) -> {
switch (code) {
case 0 -> log.info("Authentication successful");
case 1001 -> log.error("Token expired (should not occur, SDK auto-refreshes)");
case 1004 -> log.error("Signature verification failed, check appKey / appSecret");
case 5 -> log.error("WebSocket handshake failed");
case 6 -> log.error("Unknown exception: " + msg);
default -> log.error("Authentication error: code={}, msg={}", code, msg);
}
});
Returning Business Errors via Response
When SDK-side processing fails, notify the robot via response.onError():
java
@Override
public void onRequest(String agentId, String eventId, int flag,
byte[] buf, AgentParam param, Audio2LlmResponse response) {
try {
// Business processing...
} catch (Exception e) {
response.onError(eventId, 5001, "ASR service timeout");
}
}
Error Code Conventions
Error code ranges are partitioned by responsible system (which system produced the code). Integrators should branch on code, not parse message text. See dep/AgentErrorCode错误码规范.md for the full contract.
| Range | Responsible system | Examples |
|---|---|---|
| 0 | Success | Authentication success, request acknowledgment success |
| 1-999 | AgentSdk itself (never touches network) | Connection already closed, payload validation failure |
| 1000-1999 | 二开网关 (linksoul-linksky) | 1001=Token expired, 1004=Signature error, 1003=Robot offline |
| 2000-2999 | 交互网关 (aiem-emp) | Session/scheduler not found |
| 3000-3999 | Robot side | Robot execution failed |
| 4000-4900 | Integrator-defined business errors | Developer-defined, values not specified by the SDK |
Resource Release
java
// Release SDK instance (disconnect, clean up all registered callbacks and caches)
agentSdk.release();
release() performs the following:
- Sets the released flag, stops auto-reconnect
- Closes the WebSocket connection
- Cleans up callbackType registrations
- Cleans up all internal state mappings
Note: After
release(), you can callcreate()again with the same appId to obtain a new instance.
Logging Configuration
The SDK uses SLF4J + Logback. Recommended configuration:
xml
<!-- Normal operation -->
<logger name="com.agibot.aiem.sdk" level="INFO"/>
<!-- Debug message sending/receiving -->
<logger name="com.agibot.aiem.sdk.client" level="DEBUG"/>
<!-- Debug thread pool -->
<logger name="com.agibot.aiem.sdk.mgr" level="DEBUG"/>
Troubleshooting
| Symptom | Possible Cause | How to Investigate |
|---|---|---|
| Auth failed code=1004 | Wrong appKey / appSecret, or signature payload mismatch | Verify appKey / appSecret; signature payload must be "GET\n{path}\n{timestamp}\n{nonce}" |
| Connected but no messages received | Callback registered after initialize() | Ensure callbacks are registered before initialization |
| onRequest not being called | Robot not online or callbackType mismatch | Check if onRobotOnline fires |
| Response method calls have no effect | Response already cleaned up (120s timeout) | Ensure processing takes less than 120 seconds |
| Memory keeps growing | release() not called or many agentIds not going offline | Check robot lifecycle management |