Active Interaction Examples
Active Interaction Examples
v1.3.0 first exposed the active surface (alongside task flow it also shipped skill-query, state-query, pull-stream and push-listen) — but those companion entries were never functional at runtime, only task flow worked. v1.4.0 therefore removes the never-enabled entries and narrows the public surface to Task Flow (registerTaskFlow / unregisterTaskFlow); the example
directory likewise ships only TaskFlowExample.java.
Active-interaction skeleton
String url = "wss://open.agibot.com/api/V1/open-portal/app/wss/agent-sdk";
String appId = "<your appId>";
String appKey = "<your appKey>";
String appSecret = "<your appSecret>";
String agentId = "<the target agentId configured on the LinkSoul open platform>";
// Step 1: create the SDK instance
AgentSdk agentSdk = AgentSdk.create(url, appId, appKey, appSecret);
// Step 2: register the auth callback
agentSdk.registerAuth(new AgentAuthCallback() {
@Override
public void onAuthState(String appId, int code, String msg) {
System.out.println("onAuthState => appId: " + appId
+ ", code: " + code + ", msg: " + msg);
}
});
// Step 3: initialize (opens the WebSocket)
agentSdk.initialize();
Thread.sleep(2000); // wait for auth to settle
// Step 4: issue active requests (see below)
Note: unlike passive callbacks, active requests must be issued after
initialize().
TaskFlowExample — task flow (start / task / end / interrupt)
Source:
active/TaskFlowExample.java
TaskFlowRequestmodels a multi-step robot task as a pipeline:startRequest(required) →taskRequest(optional, repeatable) →endRequest(optional) →interruptRequest(optional). Each call has two-phase acknowledgement:RequestAck= the robot received the request,ExecuteAck= the robot finished that step.This example uses
"[{}]"placeholders forpayloadto keep the flow simple. Real-world payloads should follow the Task-flow payload protocol — fill inaction_group/action_typeentries there.
1) Register the task flow
String flowId = IdGenerator.generateFlowId();
TaskFlowRequest taskFlowRequest = new TaskFlowRequest(agentSdk, agentId, flowId);
agentSdk.registerTaskFlow(taskFlowRequest);
2) Interrupt (optional, callable at any stage)
taskFlowRequest.interruptRequest(new FlowInterruptCallback() {
@Override
public void onInterruptRequestAck(String flowId, String eventId, int code, String msg) {
System.out.println("onInterruptRequestAck => flowId: " + flowId
+ ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
}
}, 2000);
3) Start request (required)
String startRequestPayload = "[{}]";
taskFlowRequest.startRequest(startRequestPayload, new FlowStartCallback() {
@Override
public void onStartRequestAck(String flowId, String eventId, int code, String msg) {
// The robot acknowledged the start request
System.out.println("onStartRequestAck => flowId: " + flowId
+ ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
}
@Override
public void onStartExecuteAck(String flowId, String eventId, int code, String msg) {
// The start phase finished executing on the robot
System.out.println("onStartExecuteAck => flowId: " + flowId
+ ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
}
}, 2000);
4) Task request (optional, repeatable)
String taskRequestPayload = "[{}]";
taskFlowRequest.taskRequest(taskRequestPayload, new FlowTaskCallback() {
@Override
public void onTaskRequestAck(String flowId, String eventId, int code, String msg) {
System.out.println("onTaskRequestAck => flowId: " + flowId
+ ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
}
@Override
public void onTaskExecuteAck(String flowId, String eventId, int code, String msg) {
System.out.println("onTaskExecuteAck => flowId: " + flowId
+ ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
}
}, 2000);
5) End request (optional)
taskFlowRequest.endRequest(new FlowEndCallback() {
@Override
public void onEndRequestAck(String flowId, String eventId, int code, String msg) {
System.out.println("onEndRequestAck => flowId: " + flowId
+ ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
}
}, 2000);
Task-flow callbacks at a glance
| Callback | Trigger | Meaning |
|---|---|---|
onStartRequestAck | Start request reached the robot | code=0 means the request was accepted |
onStartExecuteAck | Start phase finished | Ready for taskRequest calls |
onTaskRequestAck | A task step reached the robot | The step request was accepted |
onTaskExecuteAck | The task step finished | Move on to the next step |
onEndRequestAck | End request processed | The pipeline is closed |
onInterruptRequestAck | Interrupt processed | The robot was told to abort |
SIMPLE vs COMPLEX
TaskFlowRequest accepts a FlowMode (defaults to COMPLEX):
// COMPLEX: start -> task x N -> end (multi-step tasks)
new TaskFlowRequest(agentSdk, agentId, flowId);
new TaskFlowRequest(agentSdk, agentId, flowId, FlowMode.COMPLEX);
// SIMPLE: startRequest carries the full payload, no taskRequest needed
new TaskFlowRequest(agentSdk, agentId, flowId, FlowMode.SIMPLE);
State listening (received via the passive callback)
State pushes have been folded into PassiveCallback.onState(...). Just override the method on
any registered passive callback — see
Passive Callbacks Guide - Shared base callbacks.
agentSdk.registerAudio2Tts(new Audio2TtsCallback(agentSdk) {
@Override
public void onState(String agentId, String eventId, String stateName, String stateValue) {
System.out.println("State change: " + stateName + " = " + stateValue);
}
// ... other callbacks ...
});