主动交互示例

主动交互示例

源码位置:agentsdk_for_java/example/src/main/java/com/agibot/aiem/active/

主动交互在 v1.3.0 起就开放了接口(一并暴露过技能查询 / 状态查询 / 拉流 / 推流监听,但这些接口实际未启用,只有任务流真正可用)。v1.4.0 把这些未启用接口从公开 API 移除,对外公开入口收敛为 任务流(registerTaskFlow / unregisterTaskFlow), 对应的 example 文件也只有 TaskFlowExample.java。

主动交互的通用骨架

java
String url = "wss://open.agibot.com/api/V1/open-portal/app/wss/agent-sdk";
String appId = "您通过灵心开放平台创建的应用获取的appId";
String appKey = "您通过灵心开放平台创建的应用获取的appKey";
String appSecret = "您通过灵心开放平台创建的应用获取的appSecret";
String agentId = "您通过灵心开放平台配置的智能体 agentId";

// 第一步:创建 SDK 实例
AgentSdk agentSdk = AgentSdk.create(url, appId, appKey, appSecret);

// 第二步:注册验签回调
agentSdk.registerAuth(new AgentAuthCallback() {
    @Override
    public void onAuthState(String appId, int code, String msg) {
        System.out.println("onAuthState => appId: " + appId
            + ", code: " + code + ", msg: " + msg);
    }
});

// 第三步:初始化(建立 WebSocket 连接)
agentSdk.initialize();

Thread.sleep(2000);   // 等待鉴权完成

// 第四步:发起主动交互(见下文示例)

注意:与被动交互不同,主动交互在 initialize() 之后才能发起。


TaskFlowExample — 任务流(启动 / 任务 / 结束 / 打断)

源码:active/TaskFlowExample.java

TaskFlowRequest 把"机器人执行多步任务"抽象成一条流水线: startRequest(必须) → taskRequest(可选,可多次) → endRequest(可选) → interruptRequest(可选)。 每个方法都有两阶段确认:RequestAck 表示请求被机器人收到,ExecuteAck 表示该步已执行完成。

本示例的 payload 用占位 "[{}]" 演示流程;真实业务请按 任务流 payload 协议 填写 action_group / action_type。

1) 注册任务流

java
String flowId = IdGenerator.generateFlowId();
TaskFlowRequest taskFlowRequest = new TaskFlowRequest(agentSdk, agentId, flowId);
agentSdk.registerTaskFlow(taskFlowRequest);

2) 打断请求(可选,可在任意阶段调用)

java
taskFlowRequest.interruptRequest(new FlowInterruptCallback() {
    @Override
    public void onInterruptRequestAck(String flowId, String eventId, int code, String msg) {
        System.out.println("onInterruptRequestAck => flowId: " + flowId
                + ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
    }
}, 2000);

3) 启动请求(必须)

java
String startRequestPayload = "[{}]";
taskFlowRequest.startRequest(startRequestPayload, new FlowStartCallback() {

    @Override
    public void onStartRequestAck(String flowId, String eventId, int code, String msg) {
        // 机器人已收到 start 请求
        System.out.println("onStartRequestAck => flowId: " + flowId
                + ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
    }

    @Override
    public void onStartExecuteAck(String flowId, String eventId, int code, String msg) {
        // 机器人 start 阶段执行完成
        System.out.println("onStartExecuteAck => flowId: " + flowId
                + ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
    }

}, 2000);

4) 任务请求(可选,可多次调用)

java
String taskRequestPayload = "[{}]";
taskFlowRequest.taskRequest(taskRequestPayload, new FlowTaskCallback() {

    @Override
    public void onTaskRequestAck(String flowId, String eventId, int code, String msg) {
        System.out.println("onTaskRequestAck => flowId: " + flowId
                + ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
    }

    @Override
    public void onTaskExecuteAck(String flowId, String eventId, int code, String msg) {
        System.out.println("onTaskExecuteAck => flowId: " + flowId
                + ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
    }

}, 2000);

5) 结束请求(可选)

java
taskFlowRequest.endRequest(new FlowEndCallback() {

    @Override
    public void onEndRequestAck(String flowId, String eventId, int code, String msg) {
        System.out.println("onEndRequestAck => flowId: " + flowId
                + ", eventId: " + eventId + ", code: " + code + ", msg: " + msg);
    }

}, 2000);

任务流回调一览

回调触发时机含义
onStartRequestAck启动请求到达机器人code=0 表示请求被接受
onStartExecuteAck启动阶段执行完成多步任务可以开始下发
onTaskRequestAck任务步骤到达机器人单步请求被接受
onTaskExecuteAck任务步骤执行完成可以继续下一步
onEndRequestAck结束请求被处理整条流水线已收口
onInterruptRequestAck打断请求被处理已通知机器人中断当前流程

TaskFlow 选择 SIMPLE 还是 COMPLEX?

TaskFlowRequest 的构造函数支持两种模式(不传则默认 COMPLEX):

java
// COMPLEX:start → task × N → end(适合多步任务)
new TaskFlowRequest(agentSdk, agentId, flowId);
new TaskFlowRequest(agentSdk, agentId, flowId, FlowMode.COMPLEX);

// SIMPLE:startRequest 自带完整 payload,不需要 taskRequest
new TaskFlowRequest(agentSdk, agentId, flowId, FlowMode.SIMPLE);

状态监听(通过被动回调接收)

状态变化推送已合并到 PassiveCallback.onState(...),直接在已注册的被动回调里重载即可,详见 被动交互指南 - 基类共享回调。

java
agentSdk.registerAudio2Tts(new Audio2TtsCallback(agentSdk) {
    @Override
    public void onState(String agentId, String eventId, String stateName, String stateValue) {
        System.out.println("状态变化: " + stateName + " = " + stateValue);
    }
    // ... 其他回调 ...
});